KOHLER Offers Ignition-Protected Starter on Expanded Range of Marine Generators

KOHLER, Wis. – April 2019 – KOHLER, a global leader in power systems, is offering an ignition-protected starter for an expanded range of its marine generators. Today, the company is rolling out an ignition-protected starter for its 14- 40EKOZD/12-35EFKOZD models, which extends the option to all KOHLER marine generators sized between 6kW and 40kW. Generators within this range are ideal for center console boats, which have skyrocketed in popularity among offshore fishermen and other pleasure-craft owners seeking a high degree of versatility on the water.

“With center consoles continuing to connect with today’s boat buyers, we wanted to expand our range of generators with ignition-protected starters,” said Patrick Kline, regional manager for KOHLER marine generators. “These 1800 RPM diesel generators can be sold as either open or closed units and are a perfect fit for the highly adaptable 38- to 60-footers with gasoline engines that are in high demand right now.”

For additional details about KOHLER marine generator for pleasure craft applications, visit www.KohlerMarine.com.

A global force in power solutions since 1920, Kohler is committed to leading-edge products and comprehensive aftermarket support. The company offers a full range of power solutions – including generators (industrial, commercial, residential, marine, and portable) automatic transfer switches, paralleling switchgear, monitoring controls and more. KOHLER marine generators are produced in the United States and distributed globally. The company’s USA, EMEA, Singapore, India, China, Australia and Brazil offices all have dedicated marine personnel supporting a network of regional distributors.

About Kohler Co. Founded in 1873 and headquartered in Kohler, Wisconsin, Kohler Co. is one of America’s oldest and largest privately held companies comprised of more than 30,000 associates. With 50 plus manufacturing locations worldwide, Kohler is a global leader in the manufacture of engines and power systems; kitchen and bath products; premier furniture under the brands of Baker and McGuire; and owner/operator of two five-star golf resort destinations which will host both the British Open and the PGA championship in 2015.

Media Inquiries

Suzanne Cutway

Director of Communications
suzanne.cutway@rehlko.com

(586) 216-3896


kohler-logo

Follow us on to find the latest updates on our products

© 2026 Discovery Energy, LLC dba Rehlko. All Rights Reserved